This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA199: 改变增益

Part Number: INA199


大家好!

我们有个项目用到了INA199A1这款放大器,但在使用过程中发现不需要50倍这么高的放大倍数,于是在IN-引脚断开与Load-的连接,在IN-与Load-串接一个51K的电阻,如下图所示。

理论上算得的放大倍数G = 1 + R1/(R3+R5) = 1 + 1MΩ/(20KΩ+51KΩ)  ≈  15倍。

但是在实际测量中,发现这样的接法放大倍数约只有3倍,不知是何原因,请指教,谢谢!

  • 您好,

    如 datasheet 中 8.4.1 Input Filtering所述,不建议这样做因为这会导致输入偏置电流不匹配 ,进而导致测量产生额外的误差。

    如果串联的话,需两输入管脚都串联,即IN+输入端也需串联同样电阻值的电阻。