Part Number: OPA810
使用该芯片做0~10V、2MHz交流信号进ADC前的Buffer,以下问题帮忙回复:
1、前端滤波使用下图手册中的阻容滤波是否可以?如果可以请问电阻和电容如何选择?
2、为了保护运放输入口,想增加一个钳位二极管,该二极管有什么要求吗?肖特基二极管是否可以?
3、使用+15V和-5V的供电方式是否可以?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA810
使用该芯片做0~10V、2MHz交流信号进ADC前的Buffer,以下问题帮忙回复:
1、前端滤波使用下图手册中的阻容滤波是否可以?如果可以请问电阻和电容如何选择?
2、为了保护运放输入口,想增加一个钳位二极管,该二极管有什么要求吗?肖特基二极管是否可以?
3、使用+15V和-5V的供电方式是否可以?

您好,
1、可以,根据所需截止频率fc设定R和C参数,fc=1 / (2πRC);
2、您是想用于哪方面的保护?下面链接是关于ESD的6个视频,您可以先了解下:
https://edu.21ic.com/lesson/2437
3、OPA810 供电电压最大支持27V,因此+15V和-5V的供电方式是可以的,但是注意其输出范围它并不是完全轨至轨输出的。