This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA810: 该芯片是否可以做0~10V、2MHz交流信号进ADC前的Buffer?

Part Number: OPA810

使用该芯片做0~10V、2MHz交流信号进ADC前的Buffer,以下问题帮忙回复:

1、前端滤波使用下图手册中的阻容滤波是否可以?如果可以请问电阻和电容如何选择?

2、为了保护运放输入口,想增加一个钳位二极管,该二极管有什么要求吗?肖特基二极管是否可以?

3、使用+15V和-5V的供电方式是否可以?