初用ths3001电流反馈性运放,datasheet上说输入电压可达4v左右,为什么我输入6M的100mv左右的正弦波,输出就已经严重失真了呢,这是我的电路图,并且放大倍数只有3倍,按反馈电阻比值应该有10倍的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电流反馈型运放对反馈电阻的要求比较高
一般情况下使用手册里面的推荐值
请参考数据手册第19页的推荐表
Table 1. Recommended Resistor Values for Optimum
Frequency Response
GAIN RF for VCC = ±15 V RF for VCC = ±5 V
1 1 kΩ 1 kΩ
2,-1 680 Ω 750 Ω
2 620 Ω 620 Ω
5 560 Ω 620 Ω
一般的关系是,使用大的反馈电阻Rf可以获得比较好的稳定性;小的Rf可以获取大的带宽
此外,你测试的时候输出端最好接一个负载电阻;例如1K