This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输出端直流分量有多大啊,你可以测 下输入端波形,查下手册看看是不是失调电压什么的原因,
在正输入端加直流偏置可以将输出直流分量抵消
你好,刚才我重新焊了一个电路,单独测试3个buf634并联构成的缓冲器,输入端和输出端波形都完美,只是输入和输出含有较大的直流分量,输入直流分量为-80mv,输出为-41mv,请问这种现象算正常吗
你好,
1、自激现象可能是因为两级级联的时候阻抗没有匹配的原因,建议你增加阻抗匹配。
2、你的信号频率是多少?要知道BUF634默认的带宽只有30M,如果频率比较大,那肯定会应为带宽的限制使得信号有一定的衰减,建议你查看634手册调整BW的相关部分,将BW拓宽,最大可以到180M
3、同时注意在进入运放前最好将直流信号进行处理,注意信号放大后的幅值与运放供电的关系。