Part Number: THS4541
如下图所示,我搭建了一个单端转差分的电路,用THS4541.
但是它的输出两端信号相位是相同的,差分之后没有幅值,请问应该怎么解决?多谢!

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在您的电路中RG是100Ω吗?这样增益是20倍。看 THS4541的datasheet,其带宽分小信号带宽和大信号带宽,您的输入信号幅值是3.3V,放大20倍,输出已超出电压供电范围,输出肯定会异常的。在大信号应用中除了考虑带宽还需考虑压摆率Slew rate满足电路要求。
看您使用了CF=2nF,这里的补偿电容一般是pF级的,不建议使用太大的补偿电容,因为这会牺牲电路的带宽。
另外,RF建议使用datasheet推荐的402Ω,使用更高的RF值会增加输出噪声,并可能会由于输入电容和反馈电阻形成的极点而降低回路相位裕度,造成电路不稳定。

输出与输入的比值小于1,这需要设置成衰减电路,衰减倍数是11倍,您将RF设置为402Ω,然后RG设置成约为 402Ω*11,测量输出信号是否为期望值?