用LM224做模拟量输入检测电路,输入电压范围是0~10V,运放输入端和输出端的电阻都采用高精度,相同温度系数,运放输出经过一个精密电阻到ADC124,运放采用单端供电方式(18V),该级电路在低温(-10℃)以及常温下(不超过40℃),模拟量输入检测正常,高温(60℃)情况下,会出现模拟量检测值逐渐减小的情况,请教该问题的解决方案。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
注意到您的电路是利用LM224做信号缩小处理,建议用电阻分压再经过LM224作为Buffer的方式。
因为LM224的手册并没有给出Bode图,无法确定在闭环增益小于1时是否会出现不稳定的状况。
Hi Jason,
这是同相放大电路,你是不是看错了 ?