电路图如上图,请问这里的跨阻放大器平稳增益的频率范围是多少?因为我感觉自己实际测得的与根据opa380datasheet给出的结果不一样,相差很大,希望能得到您的回复,还有就是我想增大带宽,该如何修改电路?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电路图如上图,请问这里的跨阻放大器平稳增益的频率范围是多少?因为我感觉自己实际测得的与根据opa380datasheet给出的结果不一样,相差很大,希望能得到您的回复,还有就是我想增大带宽,该如何修改电路?谢谢!
您好,是这样的,我用multisim 仿真时,供电电源为±5v才显示将电流信号转为电压信号,而且放大倍数与Rf一致,而当是供电电换成+5v就不能放大信号,但是datasheet写得是voltage supply 是+7v,而且实际电路中用±5v供电芯片会烧毁(已经烧毁一个了),用+5v供电能将电流信号转为电压信号,但好像带宽很小(没有实际测得,是使用者说带宽很小),之前用过ad8065作跨阻放大时就是噪声很大,带宽还基本满足要求。所以opa380在跨阻放大时应该如何接入电路才能保证带宽能到500khz呢?请教前辈
关于电源供电,请参看帖子http://www.deyisupport.com/question_answer/analog/amplifiers/f/52/t/48529.aspx中解释。
关于带宽(如果您的应用背景是光电二极管电流跨阻放大):
1.电路的连接是否正确,在OPA380datasheet的page4,page11都有相关带宽的计算公式,注意90M是增益带宽积。
2.如果你的电路带宽仿真是对的,但测试时有问题,您可以检查一下您信号源的输出信号带宽,比如对光电二极管而言,它实际上有个并联结电容,使得信号源输出信号的带宽已经衰减了。
你好,CF不知道你选用的多大,高频时建议使用较小值,比如零点几pF,电源要稳定,走线要尽量短。假设管子内阻1G,电容0.5P,可以使用1M的反馈电阻和0.3pF反馈电容可达到200K带宽
使用OPA380不可以实现你的要求,因PIN管输出电流较小,将nA级信号放大至几百mV即需要100db的放大, 而此时的OPA380实验室条件下的带宽只有200khz,不能满足您的要求。
关于互阻放大器的带宽,是与信号源电容有关的。定义略有麻烦。请参考下面的文章: