This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA280或者PGA281能否与ADS1278匹配吗?

Other Parts Discussed in Thread: ADS1278, PGA280, PGA281

信号输入带宽为20kHz,ADS1278使用的采样频率为50kHz,采用PGA280或者PGA281作为ADS1278的前端增益可调是否匹配?

1、带宽;2、两者之间能否直接连接?是否还需要加diriver?

  • 你好,不知你的增益调整范围是多少,但是PGA2870GBP为6M估计应该能满足你的需求;两者之间加低通滤波器做缓冲。你可以参考一下ADS1259EVM

  • 您好,谢谢

    1、我的增益的调整范围为1/8~128V/V(基本和PGA280吻合);

    2、你的PGA2870是指PGA280吗?

    3、是否按照ADS1259EVM设计,两者之间加低通滤波器做缓冲即可,不需要在ADS1278前增加ADC buffer?

    4、PGA280的GPIO管脚是否可以和3.3V的FPGA的IO直接连接?

    5、PGA281是否已经量产?

  • 你好,不好意思笔误写成了2870,确实是PGA280,已经量产,不需要再增加ADC buffer,可以直接和3.3V 的I/O引脚直接连接,这个是和DVDD有关的,与VSP输入无关