Other Parts Discussed in Thread: ADS1278, PGA280, PGA281
信号输入带宽为20kHz,ADS1278使用的采样频率为50kHz,采用PGA280或者PGA281作为ADS1278的前端增益可调是否匹配?
1、带宽;2、两者之间能否直接连接?是否还需要加diriver?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,谢谢
1、我的增益的调整范围为1/8~128V/V(基本和PGA280吻合);
2、你的PGA2870是指PGA280吗?
3、是否按照ADS1259EVM设计,两者之间加低通滤波器做缓冲即可,不需要在ADS1278前增加ADC buffer?
4、PGA280的GPIO管脚是否可以和3.3V的FPGA的IO直接连接?
5、PGA281是否已经量产?