INA226低边连接时负载输出是否可以接-30V电压?INA226双向电流管理是什么意思?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
nuo si 说:可是在低边输入时,VIN-接地满足要求,VIN+由于和地之间只有一个很小的采样电阻,所以承受的负电压不会太小呀?还有请解释下双向电流管理(High-or Low-Side Measurement, Bi-Directional CURRENT/POWER MONITOR with I2C™ Interface)的意思。谢谢了。
同意Curly所讲,Bi-Directional CURRENT/POWER MONITOR with I2C™ Interface,指的是可以通过I2C读取和配置寄存器的值。
双向的意思是指流经采样电阻的电流方向是双向的,也即是VIN+ - VIN- 的电压即可为正,也可为负;但有个前提,即是共模电压VCM的范围需要在0V到36V之间。
VBUS的接法是可行的,保证VBUS的工作电压范围处在0V到36V之间。
针对你的应用,Vshunt的电压较小,因此,INA226是可以满足使用要求的。另外,需要注意推荐的VCM范围是0到36V。你也可以参考LMP92064,VCM范围在-0.2V到2V之间。