Other Parts Discussed in Thread: DRV595EVM, DRV594, DRV595
drv595evm供完电源电压15v后,输出端就算是-15v,当输入端给电压信号后,输出端仍然是-15v,而且无论输入端的电压信号怎么变化,输出端都不发生变化,板子出现什么问题了?板子使用需要特别注意的地方吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.首先确认下单板的配置,如频率选择,SD,HI-Z等管脚;
2.确认下负责电阻要大于1.6 ohm
3.确认下FAULTZ的状态,如果为低的话,可能是由于OCP或者温度保护导致。
你好,
1.DRV595的输入范围是0.5-4.5V, 确认下输入信号的电平,供电电压是否都是正常的;确保信号与电源是共地的。
2.将JP3拿掉,看下FAULTZ脚的状态是否会出现低,如果为低的话 ,查找对应的可能原因