This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6644电压跟随器出现反转。

Other Parts Discussed in Thread: LMH6644

这边就是一个电压采样跟随输出的电路,前端采样经分压之后的直流电压,一旦输入超过2.6V跟随输出就出现反转输出的现象(超过2.6V,输出电压往下降),换用MCP6284没有出现此现象。运放供电是3.3V.

我用TI的TINA仿真,发现一个问题。

3.3V供电,如果输入电压2.4V, 输出2.4V ;如果输入电压2.5V,输出电压变成和供电电源一样。

4V供电,    如果输入电压3.1V, 输出3.1V ;如果输入电压3.2V,输出电压变成和供电电源一样。

也就是说,有个0.8V的压差。这个0.8V是怎么回事 ?