This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,麻烦附上电路图看下,输入信号幅值范围是多少的?
VCA821给出了不同Rf和Rg下的Gain VS Gain control voltage的曲线,比如 Figure 22是在RL = 100 Ω, RF = 453 Ω, RG = 453 Ω, +-5V 供电的条件下测试的:
当Vg=2V时,gain=2,如果按照您的测试结果,输出7.8V时,输入幅值为3.9V左右。
Vg=0.7V时,Gain=0.4,此时3.9*0.4=1.56V左右和您测试的1.9V还是有偏差的。
但是通过Gain随着Vg的增大而增大的,所以当Vg从2V到0.7V变化时,Gain是减小的,这也是为什么输出随着Vg的减小而减小的原因。
关于Vg=0.7V时,输出有很多噪声,是否还是同频率的输入条件下测试的?看起来干扰很大。
你好,电路中RL = 100 Ω, RF = 1000 Ω, RG = 10 Ω, +-5V 供电。
我的意思是Vg不仅能控制放大倍数,而且能影响到最大的输出电压。
当Vg = 2V时,最大的输出电压为7.8V左右,即使输入信号幅度再增加输出电压最大值也只能到达7.8V.
当Vg = 0.7V时,最大的输出电压为1.9V左右,即使输入信号幅度再增加输出电压最大值也只能到达1.9V.
而且Vg越小,输出信号的噪声就越大。测试时输入信号的频率为1Khz。
难道Vg能影响到最大的输出电压?
当Vg = 2V时,最大的输出电压为7.8V左右,即使输入信号幅度再增加输出电压最大值也只能到达7.8V.
VCA821不是轨至轨输出,也就是说它的输出不能达到电源轨。
可以看到,当+-5V供电时,在不同负载下的输出swing,1Kohm负载下输出+-3.9V。如果按照增益超过这个值的话,输出会削波,达到饱和,所以上一个波形中可以看到峰值有些削波现象说明输出已经饱和。
为什么有噪声,我会再看下。稍后给您回复。
VCA 821的放大倍数是2~100的范围。
按照您目前的Rf和Rg的阻值,gain=2(1000/10)=200,超过了它的增益范围,会使得它不能工作在线性范围内。
并且Rf的值您这边设置1000ohm,数据手册给出了Rf和Av的曲线,所以针对您的问题,
1.建议增益控制在100以内。
2. Rf的阻值建议根据Figure6去配置。
3.根据Rf和Rg的阻值得到最大增益2*(Rf/Rg),在这个范围内再去控制Vg的电压看是否工作在线性范围内。