由于中秋、国庆节假期,帖子审批以及工程师回复将会有所延迟,敬请谅解.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM358: 使用该芯片设计了一个差动放大电路,却无法实现预定功能?

Part Number: LM358

现在有两路方波电压信号,一路是10-0,一路是0-10,两路信号分别由H桥的左半桥和右半桥产生,相位差半个周期,占空比都为50%。

想利用LM358设计一个减法电路,将输入的两路信号变为10V的交流电压输出,供电电压为12V,单电源供电,电阻使用的是0805封装,阻值为1K。

原理图如下,为何实际无法产生10V的交流电呢?使用万用表测试大约只有1V,2V这样。