现在有两路方波电压信号,一路是10-0,一路是0-10,两路信号分别由H桥的左半桥和右半桥产生,相位差半个周期,占空比都为50%。
想利用LM358设计一个减法电路,将输入的两路信号变为10V的交流电压输出,供电电压为12V,单电源供电,电阻使用的是0805封装,阻值为1K。
原理图如下,为何实际无法产生10V的交流电呢?使用万用表测试大约只有1V,2V这样。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
现在有两路方波电压信号,一路是10-0,一路是0-10,两路信号分别由H桥的左半桥和右半桥产生,相位差半个周期,占空比都为50%。
想利用LM358设计一个减法电路,将输入的两路信号变为10V的交流电压输出,供电电压为12V,单电源供电,电阻使用的是0805封装,阻值为1K。
原理图如下,为何实际无法产生10V的交流电呢?使用万用表测试大约只有1V,2V这样。

您测试时负载是什么呢?
电路图中不建议加C1,运放驱动容性负载的能力是有限的,不建议人为加容性负载C1,否则的话可能会引起电路稳定性的问题。
在达到峰值以后,有时会出现明显的抖动,
您可以附上测量波形吗?同时告知测量时其负载是什么?
很抱歉,图片没有显示,也就是说负载是200K对地电阻?您示波器探头校准了吗?示波器测量其他正常方波效果怎样?可以正常显示吗?
我感觉输出应该可以正常显示,不该有异常,因此想让您先看下示波器探头是否有问题