之前使用PGA309 EVM,excel补偿
现在新买MULTI-CAL-SYSTEM使用自带test板时扫描0~7路时提示连接错误,电流、电压输出都一样,仔细查了接线、跳线应该都没问题,求指导一下怎么排查?感觉test上电没加上
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前使用PGA309 EVM,excel补偿
现在新买MULTI-CAL-SYSTEM使用自带test板时扫描0~7路时提示连接错误,电流、电压输出都一样,仔细查了接线、跳线应该都没问题,求指导一下怎么排查?感觉test上电没加上
您好!
不好意思,刚刚才看到您的问题。
“
对测试系统的东西不是很懂,继续请教;
今天继续试验,还是不成功,六位半我用的是安捷伦34401A,232转USB与笔记本连接,COM端口按教程改成笔记本的com4,还是连接错误。看到PPT里介绍说real RS232,real是说都是串口的么,然后又找了个带串口的本,试了下,还是通讯不上。
”
Real RS232,这么说的原因是,有些万用表后面的串口,实际上是USB-转-RS232,而不是真正的RS232接口。
如果您用的是,安捷伦的数字台表,可以用GPIB接口,Multi-Cal 软件可以支持
如果您用的是,普通国产的数字台表,一般后面的方口USB接口,实际上是串口RS232转USB,TI有更新软件支持该功能。