This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ths4509差分运放系统噪声大

Other Parts Discussed in Thread: THS4509

大家好,

    目前我的链路使用THS4509差分运放,三级放大,第一级单端转差分,50欧姆阻抗匹配,三级放大倍数依次为6dB、10dB、10dB,信号频率100MHz,系统输出噪声有10mV左右,请问为什么有这么大啊,理论上计算应该是远远小于这个10mV的,从仿真的结果来看,噪声也就在2mV左右!

    自我分析原因可能有两个:

    1、电源噪声

    2、电阻热噪声

大家帮忙分析分析!