我按THS3201的datasheet上的推荐应用电路和反馈电阻等设置的放大倍数为20倍的两级反相放大器级联的电路,当输入小于20多mv时,带宽能够达到150MHz,但是输入再增加,输出在高频的时候就失真了,输入越大输出波形越奇葩,,,我算了一下THS3201的压摆率应该足够胜任的,不知道为什么会这样?就说如何实现宽带大信号放大?原理图和PCB在下方附件的word里,急,非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我按THS3201的datasheet上的推荐应用电路和反馈电阻等设置的放大倍数为20倍的两级反相放大器级联的电路,当输入小于20多mv时,带宽能够达到150MHz,但是输入再增加,输出在高频的时候就失真了,输入越大输出波形越奇葩,,,我算了一下THS3201的压摆率应该足够胜任的,不知道为什么会这样?就说如何实现宽带大信号放大?原理图和PCB在下方附件的word里,急,非常感谢!
1.是否发热?发热需注意散热。
2.有些时候测试也有关系,注意电源,信号源,示波器的连接。
3.如果低频是好的的话,高频出现工作不正常,一般是寄生通路造成的,你可以尝试电源上加磁珠,或者阻容滤波。
1.大信号指多大?频率需要多高?
2.波形失真不单和放大器本身有关,还和电路的寄生参数有关。
3.一般研究什么问题导致的失真,可以先研究单单级的,注意阻抗匹配,包括输入和输出级,反馈电阻注意和芯片手册保持一致。
我也有大信号放大失真的问题,频段是140MHz到220Mhz左右,二次谐波和三次谐波恶化很严重,导致正弦波在示波器上看都快成方波了,输入信号2dBm的信号,放大5倍,输入输出匹配50欧姆,结果输出信号的二次谐波和基波功率只差了15dB左右,不知道为什么,还有就是3201评估板上的匹配电阻选择0805和1206封装是基于什么考虑,是输出电流吗?请指教,谢谢!