NA321的figure9 有人用过吗 真的可以实现吗 为什么我一直都没有实现放大?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
APPLICATION CIRCUITS
Medical ECG Applications
Figure 9 shows the INA321 configured to serve as a low-cost ECG amplifier, suitable for moderate accuracy heart-rate applications such as fitness equipment. The input signals are obtained from the left and right arms of the patient. The common-mode voltage is set by two 2MΩ resistors. This potential, through a buffer, provides an optional right leg drive. Filtering can be modified to suit application needs by changing the capacitor value of the output filter.
这个参考电路, 应该还有不少细节没有说到.