Other Parts Discussed in Thread: TINA-TI, INA129
用INA129的Spice模型在TINA-TI上做噪声分析,为什么TINA上分析的输入噪声频谱密度图与规格书上的不一样,整体趋势都不一样
以下为仿真电路图和TINA噪声分析结果
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在增益为0db的时候能够满足手册中给出的噪声特性,但是其他的增益的噪声特性就没有办法满足了。
通过上面的公式,我们可以换算出在100~10k段:
Vn_out=119nV/√Hz;
vn_in=7.9nV/√Hz
这样可以算出:
G=10V/V, 输入参考噪声大约为14nV/√Hz;
G=100V/V, 输入参考噪声大约为7.98nV/√Hz;
G=1000V/V, 输入参考噪声大约为7.90nV/√Hz;
看来对于这种多级放大电路构成的仪表放大器,直接通过在输入端加入噪声模块,存在缺陷。
所以仿真的时候,应该要注意这一点。