This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用OPA2335和MAX4051设计了光电二极管的前置程控放大器I-V模块,最高增益在100M和1000M的档位下数据异常,档位转换速度慢。

使用的InGaAs PIN管(-70~6dBm,响应度0.9A/W),需要放大的电流范围是80pA~4mA,放大到0-5V给AD转换器。目前测试显示最高100M和1000M档位无法测到有效数据。是不是由于运放的偏置电流过大?模拟开关的漏电流过大?或者电路本身的带宽影响了数据和速度。有没有人推荐一个运放或者电路给我。专门做光功率计(optical power meter)的前端电流放大的大神有木有,帮忙解决。