使用的InGaAs PIN管(-70~6dBm,响应度0.9A/W),需要放大的电流范围是80pA~4mA,放大到0-5V给AD转换器。目前测试显示最高100M和1000M档位无法测到有效数据。是不是由于运放的偏置电流过大?模拟开关的漏电流过大?或者电路本身的带宽影响了数据和速度。有没有人推荐一个运放或者电路给我。专门做光功率计(optical power meter)的前端电流放大的大神有木有,帮忙解决。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
使用的InGaAs PIN管(-70~6dBm,响应度0.9A/W),需要放大的电流范围是80pA~4mA,放大到0-5V给AD转换器。目前测试显示最高100M和1000M档位无法测到有效数据。是不是由于运放的偏置电流过大?模拟开关的漏电流过大?或者电路本身的带宽影响了数据和速度。有没有人推荐一个运放或者电路给我。专门做光功率计(optical power meter)的前端电流放大的大神有木有,帮忙解决。
你可以先分析一下100M欧的电阻产生的热噪声是多少,另外对带宽带来的影响。如果是手工焊的板子,一定要清洗一下。另外此时,MAX4051的关断电阻是多少,能否影响到电阻值。另外需要加倍注意PCB layout。
瞿安连教授研发的膜片钳放大器,选用的互阻抗达到50G欧。
http://cdmd.cnki.com.cn/Article/CDMD-10487-2008022773.htm
不过这时可以试一试对数放大器了