Part Number: XTR111
问题:Vin未接输入电压时,芯片输出电流34mA,使用万用表测量了以下电压:
1、测量PIN6 Vin电压,发现该引脚电压1.2V-1.5V,此时Vin未接输入信号,应当为0V
2、PIN4、PIN5分别为3V和5V,没有问题
3、PIN7,电压为8-9V,有问题,应该等于PIN6:0V
测试时,我将R9断开了,原理图和PCB如下:


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Vin高阻抗输入,不建议悬空呢,对于高阻抗输入端如果悬空的话会引起稳定性问题。
所以不建议直接悬空,接上输入信号 CTR111能正常工作吗?
接上输入信号 XTR111能正常工作了。我还想问一下,都有哪些情形下,XTR111会异常输出三十多毫安?
您好,将Vin下拉电阻到地再测试下呢?因为输入悬空条件下,以及输入会耦合进去噪声引起运放的不稳定。
另外,您说更换了一片,输出电流也是30多mA,我想可以先验证下静态电流是否符合要求。
另外,您是在哪儿购买的?