This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA 118 使用电路问题

Other Parts Discussed in Thread: INA118

各位大师,最近做了个麦克风的前置放大电路,用INA118,供电正负12V,电路图如下,因为麦克风是AC信号,用C1做了个交变耦合,R1上的电压约为1.36V, 经过C1后大约为6mv左右, 然后INA118 两个输入端分别放置了两个高通滤波, INA118放大倍数约十倍,但是不知怎么回事INA118两个输入端总是有个负高压约负11v,当敲击麦克风时,V-in 有跳变信号,这个电路用AD620后,信号可以完整的输出,用INA118后就有问题了,各位大神,帮忙看看我这个电路到底怎么回事,或者INA不V不是这样用的?谢谢了。。。

  • 你好,从电路上看不出有什么问题,能否把输入端的波形和对应的输出波形贴出来看下。

  • INA118需要在输入端提供一个共模电流回路,否则可能不正常工作。请参考数据手册FIGURE 3.

  • The input impedance of the INA118 is extremely high—
    approximately 1010W. However, a path must be provided for
    the input bias current of both inputs. This input bias current
    is approximately ±5nA. High input impedance means that
    this input bias current changes very little with varying input
    voltage.

  • 不好意思没看清楚你的电路已经有了100K的接地电阻作为输入偏置电流通路了

    那么问题有点奇怪了。你有没有试着换另一片试试呢?按照电路的配置是没错的,应该是能够正常输出的

  • 谢谢您的建议,我有两个INA118 和 两个SSM2019, 结果我通过放大信号发生器的信号发现两个INA118 坏了,一个SSm2019 坏了,放上另一个SSm2019,信号就出来了,谢谢您的帮助。。。

  • 谢谢你,我有两个INA118 和 两个SSM2019, 结果我通过放大信号发生器的信号发现两个INA118 坏了,一个SSm2019 坏了,放上另一个SSm2019,信号就出来了,谢谢您的帮助。。。

  • 请问那个1k的负载电阻是不是必须的?能删除它吗?

  • 你好,这个负载就是测试时用的,后端电路就是其负载。

  • @Andy Tan, 好的,谢谢啦。。。

x 出现错误。请重试或与管理员联系。
x 出现错误。请重试或与管理员联系。