This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位大师,最近做了个麦克风的前置放大电路,用INA118,供电正负12V,电路图如下,因为麦克风是AC信号,用C1做了个交变耦合,R1上的电压约为1.36V, 经过C1后大约为6mv左右, 然后INA118 两个输入端分别放置了两个高通滤波, INA118放大倍数约十倍,但是不知怎么回事INA118两个输入端总是有个负高压约负11v,当敲击麦克风时,V-in 有跳变信号,这个电路用AD620后,信号可以完整的输出,用INA118后就有问题了,各位大神,帮忙看看我这个电路到底怎么回事,或者INA不V不是这样用的?谢谢了。。。
The input impedance of the INA118 is extremely high—
approximately 1010W. However, a path must be provided for
the input bias current of both inputs. This input bias current
is approximately ±5nA. High input impedance means that
this input bias current changes very little with varying input
voltage.
不好意思没看清楚你的电路已经有了100K的接地电阻作为输入偏置电流通路了
那么问题有点奇怪了。你有没有试着换另一片试试呢?按照电路的配置是没错的,应该是能够正常输出的