我用LMV321做跟随器 电源3.3V 输入电压0~3.3V 居然可以输出0~3.3V ,基本线性对应关系 。LMV321的输入不是要比电源-1V吗?怎么输入也可以轨至轨了?芯片丝印RC1F
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,是的,这款运放输出能轨至轨,但输入不能,2.57供电的话输入范围0.5V~2V使得LMV321达到最佳线性工作范围。
同样5V供电的话,最大输入不超过4.2V。
您有更换过一片试试吗?是在哪儿购买的?
您好,感谢您的反馈。
是的,首先您的理解是对的,建议是按照数据手册给的电气特性去使用芯片,关于LMV321的输入电压范围,这款它不是轨至轨输入,所以3.3V输入的话,如果满足其线性范围的话输入电压范围是不允许到3.3V的。
或者您也可以在LMV321的主页上申请样片验证下: