This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VCA821的级联之后带宽很窄,该怎么解决

Other Parts Discussed in Thread: VCA821

采用如下图的参数,由于输入要求为1mV~1V,要求输入方波为50MHz,所以带宽至少要100MHz。因此Rg1 Rg2选用390欧,Rf1 Rf2选用了3.9K欧。

这样测试的结果带宽很小,结果见下图。

稍微变动Rg1 Rf1 Rg2 Rf2,都产生类似的效果,出现了尖峰。方波输入则会产生振铃和其他很奇怪的现象。

例如:

Rg1=Rg2=510, Rf1=Rf2=3900,最大平坦点大约为30MHz,也出现尖峰

再加大Rf1、Rf2,则1V输入已经失真.

请问怎么解决?

PS. 可以通过分压来减小输入电压值,但是请问能很好的消除频响上的尖峰吗?但要求输入方波为50MHz,所以带宽至少要100MHz