Part Number: OPA564-Q1
Other Parts Discussed in Thread: OPA564
1. R927=47k,当R1启动时,我们可以看到OC引脚超过2V,观察到5个PWM脉冲。最大脉冲宽度约为30us。
2. R927=10K,当我们试图将OC电阻从47k降低到10k时,OC脉冲仍然存在。
请问为什么Pin 8 OC脉冲可以一直存在于这个放大器中?放大器有损坏的风险吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,OC您指的Iflag引脚对吧? 没看到电路图,R927应该是和Iset引脚接的Rset电阻吧?
过流值可以设置在0.4A~1.5A,超过设置的过流阈值,Iflag拉高。
麻烦将电路图附上看下。