OPA522手册标注电源范围是±30V,V+端是否可以供电+32V,V-端供电-15V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
2,输入±2.5V放大12倍之后是±30V,但是我的V-端供电是-15V,即使我输入-2.5V输出也不会到-30V吧
是的是的,我上面回复错误,脑袋浆糊了。
3,U11的1脚是ADC的输出脚,程序控制ADC输出电压经过U11和U20之后输出的电压不会超过-10V~+30V范围,而且输出的是直流
您的意思是说OPA552的输入范围不是图中标的±2.5V?
32V这组单独工作的话整个系统就无法使用。而且损坏情况是随机出现的也不方便单独验证。
先不要使系统工作,断开运放的前后级,仅验证OPA552放大电路,看下在此(V+=32V,V-=-15V)供电下是否损坏?如果可以正常输入和输出,说明不是此单电路的问题;看电路图这样使用是没问题的,如果和前后级一起工作就异常,那应该与输入和输出信号有关。