This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4531: 直流输入时输出产生20MHz纹波问题

Part Number: THS4531
Other Parts Discussed in Thread: AMC1200,

尊敬的TI专家们:

为了驱动28377的16位ADC,我使用了若干如下电路进行单端转差分操作。共有5个通道,其中两个SMA输入,两个AMC1200隔离运放输入,一个取自本地的3V基准经过分压和缓冲后输入。

调试时发现,两个SMA输入的单端转差分电路中的一个,无论sma接口是开路、短路、连接信号发生器输出直流电压,差分输出总是会有一个约20M、20mVp-p的交流成分。差分输出的“+、-”端该交流成分相位差约90度。

另一个SMA通道,差分“-”端有类似的,20mVp-p但是频率为18M的交流信号,而“+”端没有。其他的通道都没有发现类似情况。请问这个信号产生原因可能是什么?应该如何消除?

整个电路电源目前由TPS8A7001将USB的5V降到3.3V供给模拟电路,四层板,模拟地和数字地分割,通过一磁珠连接。整个PCB上只有晶振工作在20MHz,且晶振离这些模拟电路距离较远。

  • 您好,

    感觉是耦合的高频干扰,TPS8A7001 是LDO还是开关电源?若是开关电源的话,其开关频率是多少?或者您测量下运放 THS4531供电电源的纹波频率看是多少?有可能是从供电电压中耦合的高频干扰。

    为排除晶振影响,您可以停止晶振工作吗?或拆掉晶振,再对THS4531进行测量?

  • 感谢您的回复!

    7A8001是一个LDO,电源没有检查到有明显的纹波峰。

    我昨天又检查了一下,发现R38右侧引脚有一些虚焊。直流测试没问题因此之前没往这个方面想。现在看也许是晶振的机械振动耦合了?或自激了?另一个通道(只有“-”端有干扰,“+”端没有的那个)没有虚焊的问题,但我把R38焊好了以后,另一个通道的干扰也消失了,这让我感到很困惑。请问您怎么看这个情况呢?

  • 您的意思是解决R38虚焊问题后,两个通道的高频振荡同时解决了?如果是这样的话,也许是虚焊的那个通道的高频振荡耦合到了没有虚焊的那个通道,使得虚焊通道问题解决后,同时也解决了没有虚焊的那个通道。

  • 可能是,但是为何两个通道干扰频率不同呢?