Part Number: THS4531
Other Parts Discussed in Thread: AMC1200,
尊敬的TI专家们:
为了驱动28377的16位ADC,我使用了若干如下电路进行单端转差分操作。共有5个通道,其中两个SMA输入,两个AMC1200隔离运放输入,一个取自本地的3V基准经过分压和缓冲后输入。

调试时发现,两个SMA输入的单端转差分电路中的一个,无论sma接口是开路、短路、连接信号发生器输出直流电压,差分输出总是会有一个约20M、20mVp-p的交流成分。差分输出的“+、-”端该交流成分相位差约90度。
另一个SMA通道,差分“-”端有类似的,20mVp-p但是频率为18M的交流信号,而“+”端没有。其他的通道都没有发现类似情况。请问这个信号产生原因可能是什么?应该如何消除?

整个电路电源目前由TPS8A7001将USB的5V降到3.3V供给模拟电路,四层板,模拟地和数字地分割,通过一磁珠连接。整个PCB上只有晶振工作在20MHz,且晶振离这些模拟电路距离较远。