Other Parts Discussed in Thread: PGA309
传感器信号电平+/-0.3uV~+/-6V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,您打算双电源供电还是单电源供电?单电源供电也有输入能允许低至-0.1V左右的,但是需要轨至轨输入。
所以相比之下建议使用双电源供电。
另外,传感器信号频率多大?需要放大多少倍?从而确定下芯片的带宽。
您好,我看了下PGA的选型,如果满足增益要求,输入信号如果为+/-0.3uV~+/-6V,那么供电至少要达到12V的,但是如果程控放大能达到128,512的话,共i供电基本在2.7V~5.5V范围。 比如PGA309这款器件,前端PGA的增益能达到128,输出输出运放的增益又可以配置为2, 2.4, 3, 3.6, 4.5, 6, 9。所以是可以实现放大倍数。您可以参考下它的数据手册:
https://www.ti.com.cn/cn/lit/ds/symlink/pga309.pdf