Part Number: INA240
Other Parts Discussed in Thread: ADS8341
如下图所示:我想达到的目的是当差分输入为0V,INA240A1输出2.5V基准电压。当差分输入大于0V,就输出大于2.5V的某个电压。当差分输入小于0V,就输出小于2.5V的某个电压。
ADC_IN0+和ADC_IN0-直接连接到AD8341的差分输入端口。这样就能直接测量出R=0.1欧这个电阻的电压。 这个设计对吗?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
在您的应用中, INA240的最大共模输入电压是24V是吗?如果是的话,那就没问题。 INA240的共模输入范围是–4 V to 80 V。
如下图所示:我想达到的目的是当差分输入为0V,INA240A1输出2.5V基准电压。当差分输入大于0V,就输出大于2.5V的某个电压。当差分输入小于0V,就输出小于2.5V的某个电压。
这样应用 INA240没问题。
INA240输出您是预打算接ADC芯片吗?我查AD8341这个型号好像不是ADC芯片?这里需要您确认的是INA240的输出电压范围需在后级芯片输入范围内。
与下面帖子是同一个问题,我将再下面链接跟进,这个帖子先关闭了,后续追问请在下面链接跟进:
https://e2echina.ti.com/support/amplifiers/f/amplifiers-forum/776344/ina240-ina240