Hi Amy Luo
我们回板调试发现INA226读取电压的寄存器无变化,能帮我们看看软件的配置嘛,下面是原理图。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
测量的直流电。
测量直流电的话,VBUS电压寄存器值就是应该无太大变化的。如果是交流电,那么VBUS电压寄存器值才是变化的。
感应电阻两端的电压比如配置0.5V和2V
那么流过采样电阻5mΩ的电流将是(2V-0.5V)/0.005=300A,根据datasheet 公式1和公式2,Current_LSB 选择 0.5mA是不可以的。