在小信号放大中(信号频率1KHz),输入信号的幅度为1uV,通过NE5532低噪放级联放大使得最终输出电压幅度达到1V左右设计的图纸如下
其中Amp1_IN是输入,Signal_Channel_3是最终输出。
在调试过程中发现运放有很高的直流偏置电压,Signal_Channel_3出无信号输出?请问是什么问题。
是不是可以采用下面的电路结构进行级联
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
偏置电压应该主要来自失调电压的影响,对于微弱信号的放大,建议前级采样仪表放大器。http://www.ti.com/lsds/ti/amplifiers-linear/instrumentation-amplifier-products.page
There is no DC path for your coupling capacitor C1 and C2. Bias current from pin3 will charge them up to rail. you need to add resistor between pin3 and GND.
赞同Yimin的说法,交流耦合为直流信号提供个返回路径是很有必要的,输入偏置电流会对耦合电容(C1 和 C2)充电,直到它们超过输入共模电压为止。不同方向的输入偏置电流,电容会充到VCC或低至地。