Part Number: PGA309
请问,我的设计中,输出级放大器放大倍数为9,输出反馈电容为47uF时,理论带宽为105Hz,但实际测量好像只有50Hz,我又试了33nF,理论带宽150Hz,实际测量只有70Hz左右。这会是什么原因造成的,为什么带宽测量值跟sboa110a中的计算值对不上。 另外,PGA309的其他信息,前级PGA放大倍数为128,GAIN DAC为0.5
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输出级放大器放大倍数为9,输出反馈电容为47uF时,理论带宽为105Hz,但实际测量好像只有50Hz,我又试了33nF,理论带宽150Hz,实际测量只有70Hz左右。
您好,您是如何测量的呢?sboa110a计算的是滤波器的带宽。比如GAIN=9. 20log9=19dB.
滤波器的截止频率为-3dB带宽,您测量下来也就是说16dB带宽处为50Hz,是这样测量的吗?
另外,您提到仿真是一致的,我没有找到PGA309的spice model。您是用TINA仿真的吗?
仿真时输出幅值为多大?实测带宽不够时的幅值为多大。我看了下PGA309的输出级压摆率只有0.5V/us。所以我想您实测带宽不够的原因很可能是收到了压摆率的影响。
没用PGA309的模型,随便找了一个运放,带宽为2MHz,而且只仿真了输出级。
是的,我想用PGA309用Tina仿真下-3dB的带宽,没找到它的仿真模型。
那电测试的方法,测试滤波器的带宽是正常的。
您好,抱歉由于元旦的关系回复迟了。
节前我将您的问题提交到英文E2E了,已经给出回复您看下,有几个问题需要您提供下,您可以直接在上面跟进,也可以在这里跟进,我去翻译:
https://e2echina.ti.com/support/amplifiers/f/amplifiers-forum/795138/pga309-pga309
抱歉,我把链接贴错了,英文链接如下,可以直接跟进,也可以发到这我来跟进。
需要提供原理图,是否输入输出有加滤波器导致了信号衰减?如何测试的带宽(带宽测试按照您的描述附上了,可能需要详细的测试方法)。另外就是提供输入输出的波形看下。
Can you provide a schematic of your PGA309 circuit? Do you have any input or output RC filters that could be attenuating the signal?
How are you measuring the bandwidth? Can you provide scope captures of the input and output waveforms?