This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA309: PGA309带宽理论值与实测值差异很大

Part Number: PGA309


请问,我的设计中,输出级放大器放大倍数为9,输出反馈电容为47uF时,理论带宽为105Hz,但实际测量好像只有50Hz,我又试了33nF,理论带宽150Hz,实际测量只有70Hz左右。这会是什么原因造成的,为什么带宽测量值跟sboa110a中的计算值对不上。 另外,PGA309的其他信息,前级PGA放大倍数为128,GAIN DAC为0.5