This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的TI工程师您好
如图所示,我需要将4-20ma的传感器输出的电流信号转换为1-5V的电压信号,然后进入ADC进行采集,我根据模拟工程师手册推荐的使用LM7322运放作为电压跟随器,使用250Ω的采样电阻,LM7322使用5V和0V的供电,由于是轨到轨的运放,LM7322输出是否能够输出1-5V,同时,后续的ADC芯片有没有推荐的,我根据 TIDA-00457的参考设计,选用ADS1220作为后续的ADC是否可以
其次,LM7322的out a输出后对于电阻和电容的配置是否需要根据ADC来计算,还是有推荐的配置电阻电容
LM7322输出是否能够输出1-5V,
您好,LM7322是轨至轨输入输出的运放,单电源供电的话,输入可以低至-0.3V,所以输入1~5V是没问题的。
输出也是轨至轨,但是输出不是绝对的能达到电源轨,大概离电源轨有几十mV的headroom。如下。 所以5V供电,输出大概在4.95V左右,所以如果需要1~5V输出,建议供电电压稍微大一些。
那么关于ADC的选择,主要考量几个参数,比如ADC的通道数,采样率,分辨率,以及接口类型比如需要SPI还是I2C,ADC的输入单端还是差分。
您选的这几款就分别是24bit, 18bit和16bit的分辨率,看您的实际需求来具体选择哪一款哈。
关于ADC,通道数是1-4都可以,采样率没有要求,分辨率在16位以上,接口类型SPI,IIC,单端输入或是伪差分输入,我重新修改了内容,您看是否可以适用
这个条件的ADC的话,这几款ADC都是合适的,3.3V 供电没问题,输入电压范围基本上都是在GVDD~VDD范围。
就看自己选择16bit还是24bit 了,可以考虑使用ADS1220.
您好,我看到您相同问题,我同事在帮您回答.如果还有其他问题,再联系。