Part Number: TLV9061-Q1

电流输出不准,最大偏差到1A,峰值输入电流30A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
C86是运放的容性负载,运放驱动容性负载会降低电路的稳定裕度。
实际负载电流和输出模拟量测算不准确。
实际负载电流是多少?测量的是直流电流吗?流过采样电阻R104的电流是多少?您搭建的相当于12倍同向比例放大电路,运放同向端实际测量电压多少?采样电阻R104是1mΩ吗?为什么右下角公式中是0.002?
对应的输出电压实际测量是多少?测量位置是运放输出管脚吗?还是R103C84滤波电路后面测量的输出电压?
您可以测量直流电流吗?然后看误差是多少?这样可以排除IGBT控制及其他因素的影响。
希望您给出更多的测试条件和测试结果的信息,这样便于我们着手去分析问题:
流过采样电阻R104的电流是多少?您搭建的相当于12倍同向比例放大电路,运放同向端实际测量电压多少?采样电阻R104是1mΩ吗?为什么右下角公式中是0.002?
对应的输出电压实际测量是多少?测量位置是运放输出管脚吗?还是R103C84滤波电路后面测量的输出电压?