This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6624: 采样问题+四线测量+阻抗匹配

Part Number: LMH6624


大神们,有四个问题想请教,关于LMH6624等运放的应用、四线测量与阻抗匹配:

(1)对应问题1,采用低端差分采样采100KHz输出电流,请问运放的电源供地是DC/DC的功率地PGND合适,还是运放后接DSP的信号地GND合适。(PGND和GND有通过0Ω电阻单点接地)

(2)对应问题2,采集1MHz开关频率的电感电流,请问运放的电源供地是功率地还是后接的DSP的信号地(和问题(1)一样,只不过开关频率更高);我接了功率地PGND,电感后的采样电阻两端电压如示波器图,蓝色是电感电流,黄色是运放采样调理后,我认为是由于采样电阻的两端寄生电感较大,导致V=L*di/dt较大,所以会有电压跌落。

(3)对应问题3,四线测量电池两端的纹波电压,非DC=3.7V的分量,纹波电压非常小可能只有10mv左右,请问四线中的(2)(3)线粗细和长短有什么要求吗,按照线路杂散电感考虑,这两条线应该越短越粗,杂散电感越小,这样考虑是否正确。

(4)对应问题4,运放采样输出的信号要传输给比较器,运放输出端和比较器的输入端距离非常近,是否还需要加R1电阻(好像是叫端接电阻,为了阻抗匹配,但是不明白算这个阻值)如果需要加R1,怎么取值呢;比较器另一端接DSP给的DAC,距离较远,大概有10cm,是否需要R2这个电阻,又该怎么取值呢。

  • 您好,

    1、我认为接PGND合适,因为被采样电路和运放都属于模拟电路,而DSP 属于数字电路,数字地和模拟地通过0Ω电阻单点连接。

    如果被采样电路是大功率信号,那么也建议通过0Ω电阻连接PGND,这样相当于三类地信号,一类功率地,一类模拟地,一类数字地,然后分别通过两个0Ω电阻连接。

    2、这里的电感是DCDC开关电路中的电感是吗?电感电流流通的回路是什么?需要考虑的是被测电路的回路要与运放共地。

    看附图波形中电感电流与运放输出波形不一致,运放输出不是期望的输出,测量电感电流的话运放输出波形与电感电流波形一致才行。

    3、 没明白③中线路的工作原理,为什么3.7V电池电压与DCDC并联?

    这两条线应该越短越粗,杂散电感越小,这样考虑是否正确。

    是的,走线越短越粗杂散电感越小。

    4、您是指比较器两输入端的匹配度吗,建议看下面博客文章的第10部分,即如下截图,然后决定是否加R1

    The Signal e-book: 有关运算放大器设计主题的博客文章汇编

    R2应该是不需要的,走线长本身会有一定的电阻,加R1是为了匹配这个走线电阻。

  • 十分感谢您的解答,针对您的解答我重新阐述下您的意思:

    针对问题(1),您说被采电路的大功率信号是什么意思,如图那种低端采样,留过电流很大,如果Rsense也很大大的话,是不是就算大功率信号了。另外,理解了您说的针对这种情况下,PGND是功率地,运放电源模拟地,后接DSP的数字地,三个地通过两个0欧电阻相连。

    针对问题(2),是buck电路中的功率电感,他的电流流通回路就是功率地PGND,所以应该就是我说的采样电阻两端杂散电感的原因。

    针对问题(3),可以认为成我想给电池充电····

    针对问题(4),我是用的专用比较器LTC6752,不存在反馈,理解为R1就是为了给R2匹配,走线电阻很小,所以认为可用0欧直接替代。