This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问关于OPA2354的供电问题

Other Parts Discussed in Thread: OPA2354

官方手册上供电范围是2.5V到5.5V(或者正负1.25V到正负2.75V),供电电压超过7.5V会造成永久损坏。
从5.5V到7.5V这段电压并没有相关数据,请问如果OPA2354工作在这段电压比如正负3V供电会有什么影响。

  • 你好,不建议在应用中时试探器件的极限,手册中的各种测试数据都是按照推荐的工作条件下得到的。

    采用+-3V的供电,会带来什么问题是不可预知的,至少我觉着会影响寿命。

  • 是否可以这么理解?
    电压超过7.5V确认会损坏,2.5V到5.5V时手册中给出的器件性能可保证。5.5V到7.5V电压范围是不确定的,性能能否保证,芯片是否损坏都是不可预知的。

  • 超过7.5V肯定会损坏,5.5V~7.5V之间性能也不敢保证,可能在这个范围内,器件仍能正常工作,那是因为在厂家一般都会留有一定的余量,但是也可能会损坏器件,所以在使用时,建议按照数据手册中“RECOMMENDED OPERATING CONDITIONS”里的参数来使用保证最佳性能。