官方手册上供电范围是2.5V到5.5V(或者正负1.25V到正负2.75V),供电电压超过7.5V会造成永久损坏。
从5.5V到7.5V这段电压并没有相关数据,请问如果OPA2354工作在这段电压比如正负3V供电会有什么影响。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
超过7.5V肯定会损坏,5.5V~7.5V之间性能也不敢保证,可能在这个范围内,器件仍能正常工作,那是因为在厂家一般都会留有一定的余量,但是也可能会损坏器件,所以在使用时,建议按照数据手册中“RECOMMENDED OPERATING CONDITIONS”里的参数来使用保证最佳性能。