This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA365: 输出振铃

Part Number: OPA365


我用OPA365搭一个减法电路,同相端口VG1是一个低电平2V,高电平5V的方波,反相端Vs2是一个要减的2V。如图。

方波频率在80kHz,输出端口电压确实被减掉了1.9V,但是产生了很大的振铃。如图(ps:自己没拍图片,但跟这个振铃图一样。)选的电阻R1=R2=R3=R4=1K,因为仿真来看1K是过冲跟振铃较好的。这种问题应该怎么分析,或者怎么解决。