This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA283: 为什么改变了原电路电压

Part Number: INA283


如图,当INA283电压V+为0时,测量点1电压为15V,但是当电压V+ > 0时(2V到18V都测过),测量点电压为13V,改变了原电路的电压,求解惑应该怎么办才能不影响原电路电压,

当48V电压没有,V+为5V时,测量点电压为0.6V

  • 1.电流检测功能是否准确?

    2.请详细描述待测电路,48V经过2个LED电压为何会只有15V?

    3.“当48V电压没有,V+为5V时,测量点电压为0.6V”,反应输入阻抗过大的情况,仍然需要描述待测电路。

  • 1.电流检测数据是对的

    2.两个led只是示意,一共12个led灯,,,,48V经过led,再经过采样电阻,这时通过运放形成了回路,LED上电就亮,这是错误的,,实际应该通过电感和驱动芯片pwm控制led亮度,结果现在上电就亮

    3.是我没接任何电路,将芯片V+,ref1接5V,gnd接地,ref2接地,这是量的+IN和-IN有电压,接近1.2V

  • C111没焊测的,,

    因为有通路,所以怀疑可能是ref这里接地的问题,,输入路和反馈路上的电阻未知,ref采用的33.3K欧的电阻,我在ref脚上飞线接了33.3K欧的电阻再接地,led不亮,,将ref1,2都接V+,led也不亮,,所以确定是这里电阻太小的问题,导致电流大了一点,使led点亮,,现在就是方案一多加电阻,但可能导致正负输入电阻不一样,会导致最终输出不稳定,待测,,,方案二都接V+,最终输出变成Vout+(Vref1+Vref2)/2,起点就5V了,超出我了的AD采样电压,,,所以还是先测方案一,,正负反馈端的电阻相等的话,包不包含ref端的电阻