如图,当INA283电压V+为0时,测量点1电压为15V,但是当电压V+ > 0时(2V到18V都测过),测量点电压为13V,改变了原电路的电压,求解惑应该怎么办才能不影响原电路电压,
当48V电压没有,V+为5V时,测量点电压为0.6V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
C111没焊测的,,
因为有通路,所以怀疑可能是ref这里接地的问题,,输入路和反馈路上的电阻未知,ref采用的33.3K欧的电阻,我在ref脚上飞线接了33.3K欧的电阻再接地,led不亮,,将ref1,2都接V+,led也不亮,,所以确定是这里电阻太小的问题,导致电流大了一点,使led点亮,,现在就是方案一多加电阻,但可能导致正负输入电阻不一样,会导致最终输出不稳定,待测,,,方案二都接V+,最终输出变成Vout+(Vref1+Vref2)/2,起点就5V了,超出我了的AD采样电压,,,所以还是先测方案一,,正负反馈端的电阻相等的话,包不包含ref端的电阻
,