Part Number: OPA2189
Other Parts Discussed in Thread: OPA2192, OPA2140


OPA2189最大输出电压幅度与频率间的关系,见OPA2189数据手册图7-36,我理解的意思是,频率在100kHz左右,OPA2189最大输出电压幅度会明显衰减不足5V。
1、我的理解是否正确?
2、见图一设计电路仿真:运放供电±5V,输入源±2.5V,仿真结果200kHz,运放输出幅值都没有衰减。与手册图7-36参数不符,让我很困惑。
3、设计的adc采集模块用到OPA2189作为低通滤波,我们需要采集至少达到200khz的信号。目前样品实测100khz复制没有衰减。手册图7-36让我很不放心,此芯片是否可以达到200khz输出5V的幅值?我是否能够继续选型此芯片。
4、图7-36,我理解没错的话,造成如此之低的原因是什么?带宽14M,压摆率20V/us,参数不低啊,请解释一下。与OPA2140/OPA2192带宽和压摆率相似的情况下,此参数相差甚远。