This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB2ANY: connect error issue

Part Number: USB2ANY
Other Parts Discussed in Thread: ALP

 when LaunchPAD shows the hardware connection, what state should the USB2ANY light be in, always on, blinking or off. Secondly, the configured setting information is not consistent with the displayed device information: the picture is as follows:

I want to connect the divice DS90UB947 ,Why does it show the message 925 ?

  • Hi,

    The content of this post is similar to your question, please see if you can refer to it.

    e2echina.ti.com/.../usb2any-usb2any


  • Hi  Why is there no Scan connected devices option in my interface? 
    my software version as follows:

  • Hi, 

    What USB2ANY hardware are you using? Are you connecting to an EVM or customer board with external USB2ANY controller? 

    If I recall, normal status should be green blinking. 

    Normally for issues like you are describing, there is no I2C communication which can result in ALP showing garbage/incorrect device information, etc. 

    Can you confirm there is successful I2C transactions between the USB2ANY and target device via logic analyzer or scope?

    Regards,