This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB2ANY: USB2ANY

Part Number: USB2ANY
Other Parts Discussed in Thread: ALP,

您好!按照链接我将固件升级,并且显示硬件连接成功 但是并没有显示954且也没有Margin Analysis界面,可能是什么原因呢,谢谢!

  • 您好,当954EVM板子和PC接上后,在PC的设备管理器中能识别到吗?

    我看您截图附上,ALP的版本没问题,USB2ANY这里也能正确识别。 在information这里,往下拉看到scan Connected devices。 点击这里,如果连接好的话会出现已连接的设备。

  •  您好,咨询一下,我们使用的设备是953和954,为什么连接成功后,显示的是925和926呢

  • 您好,按照下面这个步骤试试:

    1) Click on USB2ANY/Aardvark Setup, a new window will open.
    2) Chose the existing device, in the left hand side box, and click Remove.
    3) Under “Select a Daughter Board" search for the required device profile, in this case DS90UB954, and click “Add” and then “Ok”.

    另外,参考下UB924 的EVMuser's guide的ALP的trouble shooting的1.12.1部分ALP Loads the Incorrect Profile的步骤:

    www.ti.com/.../snlu208.pdf

  • 您好 问题已经解决了 非常感谢您的指导 谢谢!

  • 不客气,那我就把这个帖子关闭了,后续有什么问题,再讨论。

x 出现错误。请重试或与管理员联系。