This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR111: XTR111无输出

Part Number: XTR111

你好,请问问下

1.图中标黄的这句话意思。是直接理解为OD没有什么用吗?

2.如下图

这个典型应用中,有一块板子无输出,我维修时找不到问题。

查的情况如下:供电电源正常,焊接目视无问题,IC输出的基准3V在误差范围,Q1\Q2型号焊接正常,但是EF上的断线故障灯LED1常亮,实际上Iout对地接100R电阻着,即使直接对地短路,也不会灭,

另外3脚VG测试14V左右,关键2脚IS电压对地为0V,有点怀疑是IC关闭状态。

还能排查什么?